Cancel
Showing results for 
Search instead for 
Did you mean: 

Change axis resolution in FEM analysis

Experimenter
Experimenter

Hi

I made a FEM simulation of a wave washer. To set some constraints I made some small auxiliary structures. Now I have the problem that stresses at the constraints are much higher than in the rest of the part. Has anybody an idea how one can zoom in that it is possible to see also low stresses? And how can i check strains/stresses in a single element? I am using NX 9.

Thanks for your help.

2 REPLIES
Highlighted

Re: Change axis resolution in FEM analysis

Phenom
Phenom
You have come to the Femap forum instead of the NX forum, so you may want to post your question at the NX forum, as the NX people are probably not looking at these posts.

Re: Change axis resolution in FEM analysis

Experimenter
Experimenter

Thank's for thi info.

Best regards