Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Contact using elements rather than surfaces

Pioneer
Pioneer

    When I use surface to surface contact everything works ok.  When trying to generate contact connections specifying plate elements for regions it doesn't seem to work.  No error messages, no contact, elements penetrate each other as if no contact were present.

   Any suggestions. The current state of the model doesn't have useful surfaces for this.

Eli

5 REPLIES

Re: Contact using elements rather than surfaces

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Eli,

This could be something related to Shell normals of plate elements:

  • You need to make sure that all elements normals belonging to the same region (either SOURCE or TARGET) are consistently oriented in the same direction.
  • To see Element directions click F6 > LABELS, ... > SHOW DIRECTION = ON > NORMAL STYLE = NORMAL VECTOR
  • To modify element direction use command "MODIFY > ELEMENT UPDATE > ORIENT PLATE NORMAL"
  • Also the contact PAIR regions of the connector should point in opposite direction, one arrow to the other.
  • And very important, the region should be continuous, not islands of elements allowed, not isolated element plates should exist in the same region, OK?.

element-directions.png

 

If problem persist post your FEMAP model and we can take a look to it.

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Contact using elements rather than surfaces

Pioneer
Pioneer

Thanks,  I'm familiar with element orientation.  Might be the "islands".  Separate areas in surface regions are ok.  There are two separate "islands" of adjacent elements in this region.

Re: Contact using elements rather than surfaces

Pioneer
Pioneer

Removing islands worked.  anybody know why elements works different than surfaces in this regard?

Thank you.

Re: Contact using elements rather than surfaces

Pioneer
Pioneer
How do you paste images into the post?

Re: Contact using elements rather than surfaces

Legend
Legend

 

 

Image1

 

 

Image2.PNG

 

 

 

 

 

 

 

Seifeddine Naffoussi
SafeMecha Stress Engineering