Criteria or Contour Results display for particular set of elements

Valued Contributor
Valued Contributor

We are developing training material for internal purposes and initally set out in Femap. As far as I know, Femap does not have the ability to display either contour or criteria results for a selected set of elements like below.

 

 

dfdf.png

 

The above screenshot is from Patran. Per my understanding, to get the above result in Femap, I need to set up a group of the elements of interest and have the results displayed. This procedure becomes tedious.

 

I know Femap folks are revamping post-processing procedures in v12. Please do include the ability to achieve the above results.

 

Thanks...

3 REPLIES 3

Re: Criteria or Contour Results display for particular set of elements

Gears Phenom Gears Phenom
Gears Phenom

Yes you are right. I have the same probelm. I found the solution doing groups but as you said it is a tedious task. 

I hope the new version improve this

Re: Criteria or Contour Results display for particular set of elements

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

You need to define a group of the elements where you want to plot stress results, not need to activate it, then you can see the full model, but in CONTOUR OPTIONS select that group, then stress results will be plotted in that elements only, here you are an example:

 

plot-results-group-selected.png

 

plot-results-group.png

 

You can play with different visualization options, up to you!, for instance, I like this one better:

 

plot-results-group2.png

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Criteria or Contour Results display for particular set of elements

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Or you can play also with transparence on elements, properties or surfaces, the result is good as well, for instance here I set a 60% transparence on the set of properties where I don't want to plot stress results:

 

plot-results-group-transparence-properties.png

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/