Cancel
Showing results for 
Search instead for 
Did you mean: 

Data Surface Editor - Load Set Combination Method via Femap API

Experimenter
Experimenter

Hello,

 

I was trying to create a Data Surface by "Load Set Combination" Method via the Femap API, but it seems this method is not available. 

 

Actually it seems none of the methods are available below the pink line through the API...

Untitled 1.jpg

 

 

 

Are there any plans to implement the missing methods in near future?

 

 

1 REPLY 1

Re: Data Surface Editor - Load Set Combination Method via Femap API

Siemens Phenom Siemens Phenom
Siemens Phenom

We have been working to consolidate all Function Tables and other data like this into a single object.  You can create Load Set Combination Tables via the FEMAP API in v11.4 with the feTableData object.

 

Mark.