Duplicate Loadings

Experimenter
Experimenter

Hello,

 

We are experiencing some errors in the Femap model, the version used is 11.1.1.
The issue is that some of the load sets in FEMAP listed loads twice for the same node or element.  For example:
 
Load Set 110 - Wind Load (200 yrs) y-dir
  Load Definition 4 - Swivel Stack
Nodal Forces (on Node)
      ID  Color    Layer   Def CS       X          Y          Z         Phase
    83382    10        1        0         0.    117753.         0.         0.    
    83382    10        1        0         0.    117753.         0.         0.    

 

Is it possible to have a duplicate load in one load definition on shared nodal? or is it some kind of bugs?

 

TIA.

1 REPLY 1

Re: Duplicate Loadings

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Anne,

Try to isolate the problem using a reduced model size and post the FEMAP model here, we can take a look to it.

I will check also if when you export your FEMAP model to NX NASTRAN solver the nastran input deck is created correctly: use command MODEL > ANALYSIS > PREVIEW INPUT.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/