Cancel
Showing results for 
Search instead for 
Did you mean: 

Editing Manifold Sheet Solid ver. 12

Valued Contributor
Valued Contributor

Hello to all.
In earlier versions of Femap, some editing of the bodies was possible (offset of points, grid rebuilding)

 

(view in My Videos)


In the latest versions of Femap, it is not possible to move points, an error appears:

"36 Point (s) removed from selection. Only complete solids can be moved using this command."

How to edit solids now

6 REPLIES 6

Re: Editing Manifold Sheet Solid ver. 12

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

Yes, this is a know normal behaviour, according to FEMAP developers for FEMAP 12.0.x they decided to remove the ability to use the various “Move” commands to physically change the geometry. This functionality still exists, but you should now use the “Geometry Editing” tool with “Operation” set to “Project/Move Point” and “Project/Move To” set to “Along Vector” to accomplish the same things you could do before with “Modify > Move By > Point” and “Modify > Move By > Curve”, OK?.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Editing Manifold Sheet Solid ver. 12

Valued Contributor
Valued Contributor

Thank you for the answer. Yes, I tried to do as you said, but as a result, all mesh attributes are lost. Instead of the properties of the PLATEs, you get PLOT PLANAR elements:

 

(view in My Videos)

 

 

 

Re: Editing Manifold Sheet Solid ver. 12

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

I see the problem as well, I hope the new FEMAP V2019.1 version solve the problem. Meamwhile, delete the mesh, update the geometry using the MESHING TOOLBOX and mesh again.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Editing Manifold Sheet Solid ver. 12

Gears Phenom Gears Phenom
Gears Phenom

Hello Cfytrr,

 

I made a few macros to retrieve lost commands of FEMAP v11.4.2. You can try they. Here is my old post about these commands:

 

https://community.plm.automation.siemens.com/t5/CAE-Simulation-Femap-Forum/Move-By-Curve-and-Move-By...

 

Unfortunately issue related to the mesh attributes will be the same.

 

Best regards

 

Peter Kaderasz

Re: Editing Manifold Sheet Solid ver. 12

Valued Contributor
Valued Contributor

Peter Kaderasz

 

Using MoveByEntities.BAS allows you to move points, but after updating the mesh again we get PLOT elements, and the old mesh does not disappear.

Highlighted

Re: Editing Manifold Sheet Solid ver. 12

Siemens Phenom Siemens Phenom
Siemens Phenom

Fixed for v2019.1.  Thanks for pointing this out.

 

Mark.