Cancel
Showing results for 
Search instead for 
Did you mean: 

Element/Node Label Size

Dears,

 

I am looking for the menu where I can set the Element or Node ID label size.

 

thanks for help,

 

sonicP

6 REPLIES

Re: Element/Node Label Size

Valued Contributor
Valued Contributor

Hi,

press F6 (Or View-> Options) -> Labels, Entities and Parameters -> Label Parameters and set the Label Font.

 

Za

Highlighted

Re: Element/Node Label Size

Hi Za,

thank you - I thought so as welll…

but this Setting just sets the font size for Things like fringe scale, global csys - but not for the element numbering

Re: Element/Node Label Size

Valued Contributor
Valued Contributor

Hi,

I thought you were looking for what's shown below. Isn't it?

 

Cattura.JPGCattura1.JPG

Re: Element/Node Label Size

hallo Za,

 

yes, exactly that - but in my FEMAP the label size does not change:

 

 

Re: Element/Node Label Size

Siemens Phenom Siemens Phenom
Siemens Phenom

If that is Text you have to use the command Modify > Edit > Text select which ones you would like to edit and in the next dialog change the font size at the top right.

 

If you're editing several Text entities just by font size you can use this API. 

 

The HTML Clipboard

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim txt As femap.text
    Set txt = App.feText

    Dim tSet As femap.Set
    Set tSet = App.feSet

    tSet.Select(FT_TEXT, True, "Select Text to Change Font Size")

    While tSet.Next()
        tID = tSet.CurrentID
        txt.Get(tID)
        'Change Font ID below
        txt.FontNumber = 6
        txt.Put(tID)
    Wend

    App.feViewRegenerate(0)
    
End Sub

Change txt.FontNumber = according to this list 

FontID.png

Re: Element/Node Label Size

Siemens Phenom Siemens Phenom
Siemens Phenom

You are most likely using the "Performance Graphics" setting in preferences. In that mode, the labels are not controlled by the setting you are using. If you notice, in the dialog box you are showing, there is a button labelled "Performance Graphics Font". Press that, and set the size you want in that dialog.  It is independent from the labelling for the legends and axes.