Cancel
Showing results for 
Search instead for 
Did you mean: 

Export FNO Neutral Numbering

Creator
Creator

Is there any way to export a FNO neutral file while retaining the Output Set ID. I am working on a project with 500 load cases and we use the output (subcase) ID's to determine what the load is.  When reading in the .op2 you can retain the subcase ID and have the output set match.  I would like to do the same thing with the FNO but when I export a FNO file they all get renumbered to 1-500.

 

Thanks

-Jacob

3 REPLIES 3

Re: Export FNO Neutral Numbering

Creator
Creator

Due to the lack of response I am assuming this can't be done at this point.

 

Can I request that this functionality be added in the next FeMap release.

 

Thanks

-Jacob

Re: Export FNO Neutral Numbering

Siemens Phenom Siemens Phenom
Siemens Phenom

FEMAP development will look into updating this for a future release.

 

In the meantime, it is true the IDs are not preserved, however, the Results Set titles are.  We could do something clever as a work around via the API.  The script below will append all Results Sets titles with their IDs and then export an FNO.

 

Now, when the FNO is read into the new model, the Results IDs will be sequential, but the titles will have the information you wish to preserve.  The second API will take those titles and use them to update the IDs.

 

#1 - Append Titles

Before:

before_append.png

 

Run:

 


Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim r As OutputSet
    Set r = App.feOutputSet

    While r.Next()
        r.title += "\"+Str$(r.ID)
        r.Put(r.ID)
    Wend

End Sub

 

After:

after_append.png

 

 

#2 Write out FNO and import into desired model

** we can do this through API as well

 

#3 Get IDs from Titles and renumber:

Before:

before_renumber.png

 


Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim r As OutputSet
    Set r = App.feOutputSet

    Dim oSet As Set
    Set oSet = App.feSet

    oSet.AddAll(FT_OUT_CASE)
    oSet.Reset()
    While oSet.Next()
        r.Get(oSet.CurrentID)
        'Get the ID from title
        location = InStrRev( r.title, "\")
        stringID = Right( r.title, location-1 )
        ID = Val( stringID )

        'Renumber
        App.feRenumber(FT_OUT_CASE,-r.ID, ID )

        'Chop off ID from title
        r.title = Left( r.title, location-1 )
        r.Put( ID )
    Wend

End Sub

After:

after_renumber.png

Re: Export FNO Neutral Numbering

Creator
Creator

That is simular to what I ended up doing.  I wrote a script to renumber the output sets using just a table that ties the new ID's to the old ID's.  This one is nice as it is more universal.  

 

Thanks

-Jacob