Cancel
Showing results for 
Search instead for 
Did you mean: 

FEMAP 10 v3 imports IGS as several surfaces

Innovator
Innovator

Hi All

 

I am importing a FEMAP model ,a  revolution surface made in CATIA , that usually doesn't give out problems, but sometimes it can not import the IGES file with approapriate scale, then I have to click the Alternate botton, but without changing anythin , I can import with the right scale, but what I import is 1000 separate surfaces, how can I avoid this and import it as a single body ?

1 REPLY 1

Re: FEMAP 10 v3 imports IGS as several surfaces

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Farzad,

With CATIA I suggest to use STEP always, if possible. With IGES, if you have multiple surfaces, use command "GEOMETRY > SOLID > STITCH" to sew all surfaces together.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/