Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

FEMAP API - Exporting maximum stresses to data table

Creator
Creator

Hi,

 

I am trying to write an API that lets the user write a user selectable number of vectors (e.g. stresses) in user selectable load cases for a (large) number of elements to the data table and save that into a .csv file.

 

I can write the information to the message pane by using feAppMessage but I cannot write the same information to the data table. For some reason I am unable to get the arrays (C0 up to C6) to provide the information to the .AddColumn command of the data table.

 

I have put the code I have so far below.

 

 

Sub Main
   	' FEMAP itself
	Dim App As femap.model
    Set App = feFemap()
	' The data table
	Dim data As femap.DataTable
	Set data = App.feDataTable
	' Clear the data table as a precaution
	Dim rc As Long
	rc = data.Clear
	' Create a set to contain the selected elements
	Dim elmSet As femap.Set
	Set elmSet = App.feSet
	' Create a set to contain the output set and vector(s)
	Dim OutputSet As femap.Set
	Dim VectorSet As femap.Set
	Dim OutputVector As femap.Output
	Set OutputVector = App.feOutput

	' Some other variables
	Dim C0 As Variant
	Dim C1 As Variant
	Dim C2 As Variant
	Dim C3 As Variant
	Dim C4 As Variant
	Dim C5 As Variant
	Dim C6 As Variant
	Dim minID As Long
	Dim maxID As Long
	Dim minVal As Double
	Dim maxVal As Double
	Dim LocPath As String
	Dim CsvFile As String
	Dim fName As String

	'Get the filename and local path of the csv file
	fName = ""
	App.feFileGetName ("Export maximum vector", "Comma Seperated File","*.csv", False, fName)

	' Extract the filename and the save directory
    CsvFile = Mid(fName, InStrRev(fName, "\") + 1)
	LocPath = Left(fName, Len(fName)-Len(NastFile))

	' Catching if the user has not selected a filename or pressed cancel
	If Len(fName) = 0 Then
		App.feAppMessage(3,"Process cancelled!")
		GoTo Jumping_Out
	End If

	' Set the counter to 0
	count = 0

	' Get the maximum vector values
	If App.feSelectOutput( "Select Output Vectors", -1,  FOT_ANY, FOC_ANY, FT_ELEM, False, OutputSet, VectorSet ) = FE_OK  Then
	  If elmSet.Select( FT_ELEM, True, "Select Elements" ) = FE_OK Then
		OutputCount =OutputSet.Count * VectorSet.Count - 1
		App.feAppManagePanes ( "Data Table", 1)
		data.Lock ( False )
		ReDim C0(OutputCount) As Long
		ReDim C1(OutputCount) As Long
		ReDim C2(OutputCount) As Long
		ReDim C3(OutputCount) As Long
		ReDim C4(OutputCount) As Double
		ReDim C5(OutputCount) As Long
		ReDim C6(OutputCount) As Double
			' Go to the next output set
			While OutputSet.Next()
				VectorSet.Reset()
				' Go to the next output vector
			    While VectorSet.Next()
					OutputVector.GetFromSet( OutputSet.CurrentID(), VectorSet.CurrentID() )
					OutputVector.FindMaxMin(elmSet.ID, True, minID, minVal, maxID, maxVal)
					App.feAppMessage( FCM_NORMAL, Str$(OutputSet.CurrentID)+";"+Str$(VectorSet.CurrentID)+";"+Str$(minID)+";"+Format$(minVal/1000000, "0.00")+";"+Str$(maxID)+";"+Format$(maxVal/1000000, "0.00"))
					' Fill the array for the datatable
					C0(count) = count
					C1(count) = OutputSet.CurrentID()
					C2(count) = VectorSet.CurrentID()
					C3(count) = minID
					C4(count) = minVal
					C5(count) = maxID
					C6(count) = maxVal
					count = count + 1
		      Wend
		    Wend
		' Write the data to the data table
		Dim newColID As Long
		rc = data.AddColumn( False, False, FT_ELEM, 0, "Output Set ID", FCT_DOUBLE, OutputCount, C0, C1, newColID )
		rc = data.AddColumn( False, False, FT_ELEM, 0, "Output Vector ID", FCT_DOUBLE, OutputCount, C0, C2, newColID )
		rc = data.AddColumn( False, False, FT_ELEM, 0, "Minimum element ID", FCT_DOUBLE, OutputCount, C0, C3, newColID )
		rc = data.AddColumn( False, False, FT_ELEM, 0, "Minimum value", FCT_DOUBLE, OutputCount, C0, C4, newColID )
		rc = data.AddColumn( False, False, FT_ELEM, 0, "Maximum element ID", FCT_DOUBLE, OutputCount, C0, C5, newColID )
		rc = data.AddColumn( False, False, FT_ELEM, 0, "Maximum value", FCT_DOUBLE, OutputCount, C0, C6, newColID )
	  End If
	End If

	'Exporting the data table to a txt file
	rc = data.Save(True, fName, FSF_CSV)

	' Notify the user that the process is finished.
	App.feAppMessage(3,"The maximum stresses have been exported to " & fName & ".")

	' Specifying the goto point for exiting the sub
	Jumping_Out:

	' Clear the data table
	'rc = data.Clear

End Sub

 

Can  anyone see what is wrong here?

 

Thanks in advance.

 

Gertjan

5 REPLIES

Re: FEMAP API - Exporting maximum stresses to data table

Creator
Creator

All,

 

By bypassing the data table and directly outputting to Excel  I have made my API work how I want.

For anyone looking for a similar solution here is my code.

 

Sub Main
        ' This API lets the user export the maximum and minimum vector (user selectable) 
	' per load case (also user selectable) for a (large) number of selected elements and put them
	' in a new excel file.
	'
	'-------------------------------------- The declarations --------------------------------------
	' FEMAP itself
	Dim App As femap.model
        Set App = feFemap()

	' Create a set to contain the selected elements
	Dim elmSet As femap.Set
	Set elmSet = App.feSet

	' Create a set to contain the output set and vector(s)
	Dim LoadCaseSet As femap.Set
	Dim VectorSet As femap.Set
	Dim OutputVector As femap.Output
	Set OutputVector = App.feOutput
        Dim SetName As Results
        Set SetName = App.feResults

	' Some other variables
	Dim minID As Long
	Dim maxID As Long
	Dim minVal As Double
	Dim maxVal As Double
	Dim Row As Long
	Dim Col As Long
        Dim SNListTitle As String
        Dim VNListTitle As String

	'Dimension an Excel Application, Workbook and Worksheet. Be sure to activate the Microsoft Excel 12.0 Obeject Library in References
	Dim appExcel As Excel.Application
	Set appExcel =  New Excel.Application

	Dim wbkReport As Excel.Workbook
	Set wbkReport = appExcel.Workbooks.Add

	Dim wksReport As Excel.Worksheet
	Set wksReport = wbkReport.Worksheets(1)

	' Get the maximum vector values
	If App.feSelectOutput( "Select Output Vectors", -1,  FOT_ANY, FOC_ANY, FT_ELEM, False, LoadCaseSet, VectorSet ) = FE_OK  Then
		If elmSet.Select( FT_ELEM, True, "Select Elements" ) = FE_OK Then
			'Ask the API to create the titles in the first row of the worksheet
			wksReport.Cells( 1, 1 ) ="Output Set ID"
			wksReport.Cells( 1, 2 ) ="Output Set Name"
			wksReport.Cells( 1, 3 ) ="Output Vector ID"
			wksReport.Cells( 1, 4 ) ="Output Vector Name"
			wksReport.Cells( 1, 5 ) ="Maximum element ID"
			wksReport.Cells( 1, 6 ) ="Maximum value"
			wksReport.Cells( 1, 7 ) ="Minimum element ID"
			wksReport.Cells( 1, 8 ) ="Minimum value"
			' Set the row counter to 1
			Row = 1
			' Go to the next output set
			While LoadCaseSet.Next()
				VectorSet.Reset()
				' Go to the next output vector
			        While VectorSet.Next()
					' Get the set and vector ID's
					OutputVector.GetFromSet( LoadCaseSet.CurrentID(), VectorSet.CurrentID() )
					' Get the set and vector names
					SetName.SetTitle( LoadCaseSet.CurrentID , SNListTitle )
					SetName.VectorTitle( LoadCaseSet.CurrentID, VectorSet.CurrentID, VNListTitle )
					' Determine the max and min values per set and per loadcase
					OutputVector.FindMaxMin(elmSet.ID, True, minID, minVal, maxID, maxVal)
					Row = Row + 1
					' Write the data to the Excel
					wksReport.Cells( Row, 1 ).value = LoadCaseSet.CurrentID
					wksReport.Cells( Row, 2 ).value = SNListTitle
					wksReport.Cells( Row, 3 ).value = VectorSet.CurrentID
					wksReport.Cells( Row, 4 ).value = VNListTitle
					wksReport.Cells( Row, 5 ).value = maxID
					wksReport.Cells( Row, 6 ).value = maxVal
					wksReport.Cells( Row, 7 ).value = minID
					wksReport.Cells( Row, 8 ).value = minVal
		    	Wend
		    Wend
		    'Make the Excel spreadsheet visible
		    appExcel.Visible = True
		End If
	End If

' Cleaning up
Set App = Nothing
Set elmSet = Nothing
Set OutputVector = Nothing
Set SetName = Nothing
Set appExcel =  Nothing
Set wbkReport = Nothing
Set wksReport = Nothing

End Sub

Regards,

Gertjan

Re: FEMAP API - Exporting maximum stresses to data table

Hi Gertjan,

 

did u manage to get  a *.csv output as well?

 

regards,

 

der Rechenschieber

 

Re: FEMAP API - Exporting maximum stresses to data table

Creator
Creator
Hi Rechenschieber, I do not have a need for exporting to .csv output. However this can easily be done with the SaveAs option in VBA. Something along the lines of: 'Make the Excel spreadsheet visible appExcel.Visible = True wksReport .SaveAs "SaveToDirectory" & "WSName", xlCSV Where you have to specify the SaveToDirectory and WSName variables. Hope this helps. Regards, Gertjan

Re: FEMAP API - Exporting maximum stresses to data table

Siemens Phenom Siemens Phenom
Siemens Phenom

I think I've found the issue with your original API that could not write to the Data Table, and subsequently gave nothing to write to the .csv.  Your method to save to to a .csv was correct.

 

When  you were populating the array "C0", your method of "C0(count) = count" resulted in "C0( 0 ) = 0 ".  This is not valid.  I simply changed it to "C0(count) = count + 1" in order to allow the ID column to start at 1.

 

In addition, I changed how you dimensioned "OutputSet" to oSet.  Your oringial was creating an object with the exact same string name as the object definition.  This could not only be confusing, but lead to errors in your program.

 

When populating the .csv, this API will output everything in a straight line, comma-separated.  There are additional techniques such as copying the Data Table by each row or column, or using tools such as "Chr(10)" to get cariage return while writing strings.

 

Modified API below.

 

The HTML Clipboard

Sub Main
    ' FEMAP itself
    Dim App As femap.model
    Set App = feFemap()
    ' The data table
    Dim data As femap.DataTable
    Set data = App.feDataTable
    ' Clear the data table as a precaution
    Dim rc As Long
    rc = data.Clear
    ' Create a set to contain the selected elements
    Dim elmSet As femap.Set
    Set elmSet = App.feSet
    ' Create a set to contain the output set and vector(s)
    Dim oSet As femap.OutputSet
    Set oSet = App.feOutputSet
    Dim VectorSet As femap.Set
    Set VectorSet = App.feSet
    Dim OutputVector As femap.Output
    Set OutputVector = App.feOutput

    ' Some other variables
    Dim C0 As Variant
    Dim C1 As Variant
    Dim C2 As Variant
    Dim C3 As Variant
    Dim C4 As Variant
    Dim C5 As Variant
    Dim C6 As Variant
    Dim minID As Long
    Dim maxID As Long
    Dim newColID As Long
    Dim OutputCount As Long
    Dim minVal As Double
    Dim maxVal As Double
    Dim LocPath As String
    Dim CsvFile As String
    Dim fName As String

    'Get the filename and local path of the csv file
    fName = ""
    App.feFileGetName ("Export maximum vector", "Comma Seperated File","*.csv", False, fName)

    ' Extract the filename and the save directory
    CsvFile = Mid(fName, InStrRev(fName, "\") + 1)
    LocPath = Left(fName, Len(fName)-Len(NastFile))

    ' Catching if the user has not selected a filename or pressed cancel
    If Len(fName) = 0 Then
        App.feAppMessage(3,"Process cancelled!")
        GoTo Jumping_Out
    End If

    ' Set the counter to 0
    count = 0

    ' Get the maximum vector values
    If App.feSelectOutput( "Select Output Vectors", -1,  FOT_ANY, FOC_ANY, FT_ELEM, False, oSet, VectorSet ) = FE_OK  Then
      If elmSet.Select( FT_ELEM, True, "Select Elements" ) = FE_OK Then
        OutputCount =oSet.Count * VectorSet.Count - 1

        App.feAppManagePanes ( "Data Table", 1)
        data.Lock ( False )

        ReDim C0(OutputCount) As Long
        ReDim C1(OutputCount) As Double
        ReDim C2(OutputCount) As Double
        ReDim C3(OutputCount) As Double
        ReDim C4(OutputCount) As Double
        ReDim C5(OutputCount) As Double
        ReDim C6(OutputCount) As Double
            ' Go to the next output set
            While oSet.Next()
                VectorSet.Reset()
                ' Go to the next output vector
                While VectorSet.Next()
                    rc = OutputVector.GetFromSet( oSet.CurrentID(), VectorSet.CurrentID() )
                    rc = OutputVector.FindMaxMin(elmSet.ID, True, minID, minVal, maxID, maxVal)
                    App.feAppMessage( FCM_NORMAL, Str$(oSet.CurrentID)+";"+Str$(VectorSet.CurrentID)+";"+Str$(minID)+";"+Format$(minVal/1000000, "0.00")+";"+Str$(maxID)+";"+Format$(maxVal/1000000, "0.00"))
                    ' Fill the array for the datatable
                    C0(count) = count+1
                    C1(count) = oSet.CurrentID()
                    C2(count) = VectorSet.CurrentID()
                    C3(count) = minID
                    C4(count) = minVal
                    C5(count) = maxID
                    C6(count) = maxVal
                    count = count + 1
                    Wend
            Wend
        ' Write the data to the data table
        rc = data.AddColumn( False, False, FT_ELEM, 0, "Output Set ID",FCT_DOUBLE, OutputCount, C0, C1, newColID )
        rc = data.AddColumn( False, False, FT_ELEM, 0, "Output Vector ID", FCT_DOUBLE, OutputCount, C0, C2, newColID )
        rc = data.AddColumn( False, False, FT_ELEM, 0, "Minimum element ID", FCT_DOUBLE, OutputCount, C0, C3, newColID )
        rc = data.AddColumn( False, False, FT_ELEM, 0, "Minimum value", FCT_DOUBLE, OutputCount, C0, C4, newColID )
        rc = data.AddColumn( False, False, FT_ELEM, 0, "Maximum element ID", FCT_DOUBLE, OutputCount, C0, C5, newColID )
        rc = data.AddColumn( False, False, FT_ELEM, 0, "Maximum value", FCT_DOUBLE, OutputCount, C0, C6, newColID )

      End If
    End If

    'Exporting the data table to a txt file
    rc = data.Save(True, fName, FSF_CSV)

    ' Notify the user that the process is finished.
    App.feAppMessage(3,"The maximum stresses have been exported to " & fName & ".")

    ' Specifying the goto point for exiting the sub
    Jumping_Out:

    ' Clear the data table
    'rc = data.Clear

End Sub

Re: FEMAP API - Exporting maximum stresses to data table

Creator
Creator

Sorry for bringing up an old thread, I had similar code with the same issue when exporting into a table. The IDs for all stress values aren't shown and only a handful are displayed. For example, 15 stress IDs selected but only 10 are shown with their values. Any idea for a possible solution?

Thank you!

 

Edit: Fixed the code and followed the same approach. A problem with the code above would be not outputting the final von mises stress. I guess this is an issue with the output counter stopping before counting the last ID. A simple work around would be changing the addcolumn statements to:

 

The HTML Clipboard

 rc = data.AddColumn( False, False, FT_ELEM, 0, "Output Set ID",FCT_DOUBLE, OutputCount+1, C0, C1, newColID )