Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

FEMAP TRIAL - SOL601,N and SOL701

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello all,

Are there any solutions NOT supported with a FEMAP TRIAL license? Most solutions run (e.g. 101,106,109,129), but I get the following error message when trying to run SOL601,N and SOL701 (see below). Does this mean that FEMAP TRIAL does not include these SOL601,N and SOL701? Is there a workaround?

 

Thank you!

 

*** EXECUTE SOLUTION ***
 *** MAXIMUM MEMORY FOR ANALYSIS = 5528 MB ***
 PID=3264
 Could not check out NX Nastran Advanced Nonlinear license feature.
 return code = 1
 *** SOL 701 EXITED WITH INVALID STATUS CODE -1
 *** MOST LIKELY, PROGRAM HAS CRASHED.
 *** FATAL ERROR: SOL 701 DID NOT FINISH SUCCESSFULLY.
 *** ADVANCED NONLINEAR EXIT CODE 0 ***
 *** ISHELL PROGRAM 'NXNA' COMPLETED ***
 ^^^ USER   FATAL   MESSAGE  
 ^^^ ERROR IN ADVANCED NONLINEAR MODULE          0
 ^^^SOL701 FAILED    
1    EXPLICIT 3        

2 REPLIES 2

Re: FEMAP TRIAL - SOL601,N and SOL701

Siemens Phenom Siemens Phenom
Siemens Phenom

The Femap with NX Nastran trial includes NX Nastran Basic (Linear Statics, Normal Modes, Buckling and Heat Transfer) as well as the Dynamic Response option.

 

You can find out what options are licenses using the Help > About command.  Click the Security button in the Femap with NX Nastran dialog box, then click the Show Licenses button in the Network License Information dialog box.  That will list all the Femap licenses that you are authorized for.

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development

Re: FEMAP TRIAL - SOL601,N and SOL701

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thank you Chip. This completly answers my question.

Regards,

Jacques