Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

FEMAP material orientation problem

Experimenter
Experimenter

Hi everyone, 

 

I am currently working on my masters thesis and I have the following issue with laminate material orientation in FEMAP v 11.1.2. My model is axially symmetric, it is basically a composite aircraft wheel. It is made from UD tape, so 0° fibres are oriented radially towards the wheel axis, which is also CS's origin. I have issues while trying to orient the material towards the centre: I tried it on a simple circular plate with three plies, and it works perfectly well (Material angle - Coordinate axis - CSys - Basic Cilyndrical - R axis), but not on my model. ( I activated cylindrical CSys).

 

Any help is well appreciated,

Thanks in advance - Petar

mat_orientation.JPG

2 REPLIES 2

Re: FEMAP material orientation problem

Gears Phenom Gears Phenom
Gears Phenom

Hi Petar

 

I have seen this happen before on composite fairings. Few things you can do to help.

 

1. Align your element co ordinate systems to the cylindrical cys - do this using Modify > Update elements > Orient Plate Normal/First Edge.

 

- This will also align the element directions correctly so that post processing is easier as your direction shear is properly setup - ie you don't have to transform the results if done correctly.

 

 

CCYS.JPG

 

Next and probably more importantly you need to change the cys setup - currently you have the Z (Axial component) running in the wrong direction. I setup the above model with the CYS in the same orientation as you had and the material direction would not update correctly - once the axial component is set correctly the material direction aligned properly.

 

MAT.JPG

 

Re: FEMAP material orientation problem

Experimenter
Experimenter

Thanks a lot, this solved my problem ! 

 

Petarmat_orientation.JPG