10-10-2018 10:35 AM
With v12.0, all floating network licenses of FEMAP and FEMAP w/NX Nastran automatically include the option to borrow a license for up to 30 days. To borrow, you must be connected to your network, and able to communcate with the machine hosting your FEMAP FLEXlm license. There is a program called BORROW.EXE in the main FEMAP directory (we don't create a link to it, but probably should in the future).
Run BORROW.EXE, and enter the the name of your FEMAP License Server preceded by the "@" character, you will see something like this -
If you reconnect before the borrow expiration date, you can return the licenses early using the same BORROW.EXE utility.
The FEMAP Team
10-11-2018 03:25 AM
Hello Mark,
when will be available the floating network license to FEMAP v12? Our Hungarian reseller can't get this license from Siemens yet.
I installed FEMAP v12 a few days ago, but I can't use it, because it don't work with license to FEMAP v11.4.2.
Best regards
Peter Kaderasz