Cancel
Showing results for 
Search instead for 
Did you mean: 

Femap 11.4 bug revolution surface

Dear all,

 

I see that with new femap version, if  I revolve curve to obtain a surface, I obtain a distorted object that I can cut.

 

I attach an example of  what I obtain if I try to create a pressure vessel with curve revolution.

Can Anyone help me?

 

Best regards

Stefanovessel.PNGdistorted surface

2 REPLIES 2
Highlighted

Re: Femap 11.4 bug revolution surface

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Stefano,

FEMAP V11.4 is running OK, I have rotated curves using command GEOMETRY > SURFACE > REVOLVE and the result is correct, I can stitch the revolved surfaces and create a solid body, cut, etc,,

If I inspect your FEMAP model one think that takes my attention is that not any entity (surface or body) exist under GEOMETRY in the MODEL INFO tree!!.

If I list your surfaces using command LIST > GEOMETRY > SURFACES > ALL then I see the following:

List Surfaces
5 Surface(s) Selected...
 
     ID      Type Color Divisions <--- Curves ( R = Reversed Direction ) --->   Layer   #Volume
_______________________________________________________________________________________________
       1  Revolve    60  16 x 2          4          3          1 R                   1        0
 
       2  Revolve    60  16 x 3          6          5          4 R        2 R        1        0
 
       3  Revolve    60  16 x 2         10          9          7 R                   1        0
 
       4  Revolve    60  16 x 3         12         11         10 R        8 R        1        0
 
       5    Ruled    60   3 x 16        15         14 R       16 R       13          1        0

But if I list the surfaces in the model I have created from scratch at my end I see the following:

List Surfaces
10 Surface(s) Selected...
 
     ID      Type Color Divisions <--- Curves ( R = Reversed Direction ) --->   Layer   #Volume
_______________________________________________________________________________________________
       1     Face    58   3 x 4                                                      1        0
                 Segments:   57  Address: 1647951
 
       2     Face    58   3 x 4                                                      1        0
                 Segments:   57  Address: 1647904
 
       3     Face    65   3 x 4                                                      1        0
                 Segments:  100  Address: 1648059
 
       4     Face    65   3 x 4                                                      1        0
                 Segments:  100  Address: 1647997
 
       5     Face    72   3 x 4                                                      1        0
                 Segments:   57  Address: 1648162
 
       6     Face    72   3 x 4                                                      1        0
                 Segments:   57  Address: 1648115
 
       7     Face    79   3 x 4                                                      1        0
                 Segments:  642  Address: 1648276
 
       8     Face    79   3 x 4                                                      1        0
                 Segments:  642  Address: 1648214
 
       9     Face    86   3 x 4                                                      1        0
                 Segments:  634  Address: 1648400
 
      10     Face    86   3 x 4                                                      1        0
                 Segments:  634  Address: 1648338
 

QUESTION: wich geometry engine are you using with FEMAP V11.4?. I mean, under FILE > PREFERENCES > GEOMETRY MODEL the GEOMETRY ENGINE is 1..Parasolid or 0..Standard ??. You need to select the Parasolid engine.

Please check your options and let us know your progress, thanks!.

Best regards,
Blas.

 

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Femap 11.4 bug revolution surface

Dear Blas,

 

I solve the problem. Thanks.

 

I don't understand why in this version is setted by defaults standard geometry instead parasolid...

 

No is all ok.

 

Best regards

Stefano