Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Femap API - Skipping initial neutral file dialog when opening

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I'm trying to write an API program to open up a bunch of old Femap files and write out neutral files without the results. Whenever I open the files, it immediately opens a neutral file import dialog and asks what items should be imported. I'd like to do a bunch of these in batch mode without having to click on the dialog box for each file. Is there a way to get the API to skip that user dialog and just accept the defaults?

3 REPLIES

Re: Femap API - Skipping initial neutral file dialog when opening

Phenom
Phenom

It looks like you need to use the Femap Application -> File ->  fefileReadNeutral3 method, which allows you to set all these choices within your API.  The equivalent for exporting looks like feFileWriteNeutral2.

Re: Femap API - Skipping initial neutral file dialog when opening

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

To follow up on this, it seems that Femap uses one of the neu_*.exe neutral file converter executables on the model when it opens. Each executable only works for a certain version of Femap, so it somehow first detects the model version before running the executable. Is there a way to determine the version of a Femap file without opening the file?

Re: Femap API - Skipping initial neutral file dialog when opening

Gears Legend Gears Legend
Gears Legend

Hello,

 

I don't know, how should you check version in official way, but I found in beginning of all model file (*.mod, *.modfem) the version number from Femap v8 (in the file header). You can find string "APPL=FEMAP Version " and next you can find the version number (after SPACE character). Searching can be finished if you found string "END_OF_HEADER".

 

Text                                            - Absolut position in the file (hexadecimal)

"APPL=FEMAP Version 8.00"   - 0720H

"APPL=FEMAP Version 10.11" - 0234H

"APPL=FEMAP Version 11.11" - 0234H

"APPL=FEMAP Version 11.20" - 0234H

"APPL=FEMAP Version 11.31" - 0234H

"APPL=FEMAP Version 11.42" - 0234H

 

I think so you can identify Femap version of your models.

 

Best regards

 

Peter Kaderasz