Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Femap Version 12 Preview: Geometry Modeling

Community Manager Community Manager
Community Manager

Femap Version 12 What's New: Geometry Modeling

 

The Femap version 12 release is coming up very soon, so let’s see some of the new geometry creation and manipulation enhancements that we can look forward to.


Let's take a closer look at what's coming as far as geometry modeling updates are concerned.

 

Geometry modeling enhancements

 

Geometry stitching and combined curves and surfaces

 

Box_01_350x263.jpg

A new geometry stitching algorithm introduced in version 12 improves the performance and method by which composite surfaces are connected together. This algorithm, which uses multi-body processing controlled by a tolerance, makes it much easier to combine surfaces and composite surfaces, with overlapping edges and gaps, in a single command to create fully connected geometry that is ready to mesh.

 

Handling of combined curve and surface geometry also extends to Boolean operations, where interfacing geometry is recombined and updated automatically according to the operation undertaken. Combined and boundary curves and surfaces are preserved during solid operations and new combined geometry is created as required to maintain geometry topology.

 

Surface alignment

 

GraphicsUI_06-1_300x225.jpg

 

Femap version 12 introduces a new surface alignment command that can remedy geometry misalignment that may arise, for example when combining periodic surfaces with data imported from various CAD systems. Aligning geometry prior to meshing minimizes the creation of disruptive short edges and facilitates the generation of a good finite element mesh. The surface alignment command also includes an automatic alignment method which can be applied to all or a number of selected surfaces.

 

 

 

Surface between curves

Box_01_350x263.jpg

 

Geometry enhancements include an enhanced curve-to-curve surface connection option that extends the previous ruled connection method by adding tangent-to-surface and vector aligned options.

 

 

Performance improvement

 

The feature removal capability has been improved to maximize performance, and is now more than 30 times faster.

 

 

Watch the video below to see the new geometry modeling enhancements coming in Femap version 12.

 

 

(view in My Videos)

 

Return to Table of Contents

1 REPLY

Re: Femap Version 12 Preview: Geometry Modeling

Pioneer
Pioneer

„Align Surface Parameters” function is great! I've always had trouble with misaligned surfaces. It completely resolves this issue.

Marek