Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Glue without geometry, only mesh

Valued Contributor
Valued Contributor

I need to glue two parts together, but have no geometry definition, I only have the meshes.

I created a surface on the meshed areas to be glued, created regions and a connector but I get funny error messages. *** USER FATAL MESSAGE 4690 (SCTFCRL)
NO SURFACES OR EDGES DEFINED FOR CONTACT/GLUE REGION 6

But I have defined a surface and Glue region 6!

Is gluing with meshes possible at all this way, or do I have to create the geometry ang make a new geometry based mesh?

Rgds Bernt

3 REPLIES 3

Re: Glue without geometry, only mesh

Gears Legend Gears Legend
Gears Legend
It can be done.

How did you set up your connector regions?

Re: Glue without geometry, only mesh

Gears Phenom Gears Phenom
Gears Phenom

When you define the regions you can choose , surfaces, curves, elements.....

 

image.png

Re: Glue without geometry, only mesh

Gears Phenom Gears Phenom
Gears Phenom

I realized that maybe you have created the surfaces but you did not associate the mesh to geometry. Thus, when the file is sent to the solver it can not translat the elements/nodes attached to surfaces and the error comes out. I guess this is the problem

 

So either you perform this step or you make contacts with elements.