Cancel
Showing results for 
Search instead for 
Did you mean: 

How to control and set the nodes to specified location?

Pioneer
Pioneer

Dears, as a newbie and no many experience with FEA, please pardon me to ask these easy questions. I'm not familiar with the surface meshing, so usually I just use automatic mesh function, usually it's no problem when the loads are distruibuted on the surface, but when I try to locate the load on some specific nodes, I got problem, because there always have some deviation between nodes and the location I expected. I know there must have the way to solve this problem, but how? Can anybody do me a favour to show some details? Or is there any demo or guidance to see? Thanks indeed for any suggestion.

 

LOCATION.jpgthe location I expected. 

2 REPLIES

Re: How to control and set the nodes to specified location?

Valued Contributor
Valued Contributor

Use Mesh -> Mesh Control -> Mesh Point on Surface..

2017-02-26_20-53-47.png

Select Surface to set custome mesh and creat points where are you need.

 

Also, you can slice you surface using Geometry -> Solid -> Slice

 

Second variant is more usable. Because you can control mesh quality.

2017-02-26_21-07-39.png

Re: How to control and set the nodes to specified location?

Pioneer
Pioneer
Sorry for the late reply, yes, that is what I want, thank you so much.