Cancel
Showing results for 
Search instead for 
Did you mean: 

How to plot Frequency data on the chart

Pioneer
Pioneer

Hi,

 

I am doing Normal/Eigen Value analysis and want all the results to get plotted automatically in the chart which would give me some kind of visual aid to know the intensity related to particular frequency.

 

How can I do that.

 

Thank You

2 REPLIES 2

Re: How to plot Frequency data on the chart

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Are you refering to a frequency response analysis?  Or were you thinking of mass participation?  If the former, you'll need to run a frequency response solution with perhaps a unit input to get a sense of magnitude (assuming you don't have defined input).  I believe there are some auto-charting options offered when you right click a freq response solution's "analyis study".

 

 

Eric Gustafson

Author, Learning Femap

Re: How to plot Frequency data on the chart

Pioneer
Pioneer

Please have a look at the pic I have attached. I got to know that Mass fraction should be atleast 90% of the total. So what else can I extract from the following figure?