Interesting article about Tetra Vs Hexa Elements.

Creator
Creator

Hello everyone !

 

I found out on Google a interesting article about tetra vs hexa elements, the author compare the results performing linear and non linear analysis, compression, tension, bending, torsion, vibration and also perform real tests. It really worth it reading ! (If you are interested of course).

 

Please feel free to post your conclusion/opinion and share information !

 

Thanks !

6 REPLIES 6

Re: Interesting article about Tetra Vs Hexa Elements.

Valued Contributor
Valued Contributor

Yes, very intersting, Rodrigo! But did you also do any study on efficiency. I'm thinking about time and Computer resourses. If you have model where you could get acceptable results with say, 1 million nodes with linear Hexas, how many nodes would you require to get acceptable results with quadratic TET's?

 

Rgds Bernt

Re: Interesting article about Tetra Vs Hexa Elements.

Creator
Creator

Dear Bernt,

 

In terms of numbers i have no idea, it varies from model to model, geometry and so on, But to figure out this you have to perform a convergence test.

Gradually you will raise the number of nodes in your model and check the stress level, if the stress diference between the tests are low, you are in the sweet spot, which means you dont have to increase the number of nodes.

 

Did i answer your question?

 

Best Regards.

Re: Interesting article about Tetra Vs Hexa Elements.

Phenom
Phenom
This applies to ANSYS, not necessarily to Nastran. In particular, NX & MSC Nastran correct the issues ANSYS (and Abaqus) have with linear brick elements with a bubble function, making the CHEXA4 very efficient and accurate, far better than ANSYS or Abaqus.

We make 5-6 millions dof HEX models every day and are very good at it. It'd be much easier to do a "one click, TET mesh everything", but we'd end up with TB op2 that would bring no better insight than our HEX models... That is the point Bernt was making, I'm pretty sure he wasn't asking for a recommendation :-)

Re: Interesting article about Tetra Vs Hexa Elements.

Valued Contributor
Valued Contributor

Yes, that's true. I'm no fan of Tets, probably for no better reason than when I started usinfg FEM back in the 1980's, using Tets were banned and was not an issue. But I see the point that it is, for many geometries, much easier to mesh. But as long as I can mesh with HEXAs with reasonable effort, I tend to stick to that.

Rgds Bernt

Highlighted

Re: Interesting article about Tetra Vs Hexa Elements.

Creator
Creator

Indeed, the pros for tetra elements is that when you have complex geometry it´s almost impossible to mesh using hexa. In my point of view, banning tetra elements is a mistake, as i said, tetra elements plays an important role. But if you are able to mesh using hexa elements, of course, you should use it.

Regarding the convergence test, i wouldn´t say that, no matter what software you are using (FEMAP,ABAQUS, HYPERMESH, ANSYS...) "convergence test is the basis theory of CAE" (A. Filho, " Elementos Finitos A Base Da Tecnologia CAE ". São Paulo, Érica, 2013.

Thanks.

Re: Interesting article about Tetra Vs Hexa Elements.

Phenom
Phenom

I don't think there is anyone banning TET anymore (parabolic that is).  It was impractical decades ago because of the amount of data to deal with and computing power available, but Model Solution, NX Nastran and others have been using iterative solvers for 15-20 years, so the performance has been just fine.  The issue still remains of the size of the result sets.  There is no problem getting good results with TET10 as long as they are used properly.  Same is true for HEX to some extent, but it is so easy to generate terrible data with a TET mesh...

 

The issue is rampant laziness or ignorance, facilitated by this so-called "democratization" and the new illusion that 5 minutes on youtube and asking reddit is pretty much enough to "do analysis": as long as you can catch a few buzzwords to use in conversations to sound knowledgeable and know when to run away or pretend enough to get by...  I see it everyday and it is sad the amount of garbage being generated...  

 

The basis of FEA is Ritz, Galerkin and Euler approximation of continuum.  In other words: there is a lot of high level math involved that also comes with major caveats. Unfortunately, the "democratization" gives the illusion that understanding any of this is not neccessary...

 

Here's a great video that could illustrate my point: 

 

 

Shinji Kagawa and his teamates use bricks & TETs when it makes sense to obtain good results Smiley Happy