Cancel
Showing results for 
Search instead for 
Did you mean: 

Issue deformation on plate elements

Experimenter
Experimenter

Hi,

 

I was trying to do a 2D simulation, and in this situation I connected a RBE3 on plate element node like we can see in the picture below. When I saw the results of the simulation, the node that I connected with the RBE3 did not translate with the rest of the structure.

Note: Previously I did the simulation with the RBE3 connected in diferents nodes in this same surface and this did not happen, the node translate just a few. The loads continue the same in the two cases.

 

foto2.PNGfoto1.PNG

 

Normal deformation:

foto3.PNG

 

Thanks for your help,

Best regards,

Rogeriopq.

1 REPLY 1

Re: Issue deformation on plate elements

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Roger,

With the pictures you posted I don't have a clear idea of the exact problem, I suggest to post your FEMAP model, or define a small problem that represents the problem you have, OK?.

Best regards,

Blas. 

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/