Highlighted

LINEAR CONTACT IN NON LINEAR ANALYSIS

Not applicable
One improvent which will help a lot and make the job easier is the linear contact to work in Non Linear Analysis.
Today, we only can performance it in Linear Study or if we use the "glue" contact.

Cheers!
4 REPLIES 4

Re: LINEAR CONTACT IN NON LINEAR ANALYSIS

Innovator
Innovator
Hello!,
Next verion of NX NASTRAN V9.0 will feature a new nx nastran "native" advanced nonlinear solution sequence named SOL401, I am not sure if the initial release will support surface-to-surface contact, but will be the architecture for future extensions, very exciting!!. Alternatives: SOL106 with CGAP node-to-node contact, and learn to mesh correctly.
Best regards,
Blas.

Re: LINEAR CONTACT IN NON LINEAR ANALYSIS

Not applicable
Hi Bias,
It would be wonderful if this issue works in SOL101 like works in SOL601...it can help a lot!
Maybe in near future....
Tks,
Best Regards,

Re: LINEAR CONTACT IN NON LINEAR ANALYSIS

Innovator
Innovator
Hello!,
This will be imposible, SOL101 is LINEAR static, and SOL601 IS NONLINEAR, the solution will be the same if the model to solve is LINEAR by nature, then both solvers will arrive to the same results. I guess you are referring to SOL401 ....
Best regards,
Blas.

Re: LINEAR CONTACT IN NON LINEAR ANALYSIS

Not applicable
Yes.....you are right! In Non Linear (Basic Module).
Tks