Cancel
Showing results for 
Search instead for 
Did you mean: 

Load definition

Valued Contributor
Valued Contributor

Hi

 

I could do with some help.

I need to define a load case (Load ID) with two different laods on 2 different nodes. How can this be done in FEMAP.

2 REPLIES 2

Re: Load definition

Siemens Phenom Siemens Phenom
Siemens Phenom

Use Model->Load->Create/Manage Set and press "New Load Set" to create your load case. Then use Model->Load->Nodal, select your first node and define the load you want. Do the same thing with the second node, just define a different load. 

 

Alternatively, if you skip using Model->Load->Create/Manage Set, and don't have any Load Sets, Model->Load->Nodal will allow you to create a Set the first time it is used.

Re: Load definition

Valued Contributor
Valued Contributor
Thank you!!

That worked!!!!



Bernt Isaken

dyNOVA logo1

Dynova