Cancel
Showing results for 
Search instead for 
Did you mean: 

Load modal analisys results in dynamic analisys

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello everyone.

Basically, i have a big model with lots of elements, in which the modal analisys takes quiet too long to complete.

In this model, i need to perform some tests using time history/dynamic analisys using nodal superposition, but everytime i run a time history analisys, a modal analisys is also performed.

 

But the geometry is all the same, i am only viring some curve parameters, i don't need to run a modal analisys everytime i want to change some curve parameters.

 

I want to know if it's possible, within FEMAP, to load the modal analisys inside the dynamic. In order to save some time.

 

Best regards,

Igor Carvalho

2 REPLIES 2

Re: Load modal analisys results in dynamic analisys

Gears Phenom Gears Phenom
Gears Phenom

Yes, this is called Restart. Check Example 16. Modal Frequency Analysis of the Hinge Model in Help -> Examples.

Restart.JPG

 

Re: Load modal analisys results in dynamic analisys

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thanks, that worked.

Even though now i realized that what actually takes time is not the modal analisys, but rather the ammount of reults requested.

 

Anyway, thanks for your time.

 

Att,

Igor Carvalho