Cancel
Showing results for 
Search instead for 
Did you mean: 

Long time until analysis starting in case of Bolt Preload on Solid type Bolt Region

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

when I used Bolt Preload on Bar type Bolt Region in my model, the part of my log file war the following:

 

08:22:54 Beginning Analysis

08:22:54 NX NASTRAN Authorization Information - System Attributes
08:22:54 --------------------------------------------------------
08:22:54 Model: Intel(R) Xeon(R) CPU E5-1650 v3
08:22:54 Machine: Intel64 Family 6 Model 63 Steppi
08:22:54 OS: Windows 7
08:22:54 Version: Service Pack 1
08:22:54 License File(s): 28000@LocalHost

08:22:54 The FEMAP dll Search String is c:\femapv1132\auth_*.dll .
08:22:54 Found the FEMAP authorization dll auth_113.dll
08:22:54 Loading FEMAP Authorization dll auth_113.dll

08:22:54 NX NASTRAN Authorization Information - Checkout Successful
08:22:54 ----------------------------------------------------------
08:22:54 License for module NX Nastran Basic - FEMAP Desktop checked out successfully

08:23:10 Analysis started.
08:23:10 Geometry access/verification to CAD part initiated (if needed).

 

In this case analysis started after license checked out in 16 seconds.

 

When I used Bolt Preload on Solid type Bolt Region in my model (with tetra elements), the part of my log file war the following:

 

15:05:55 Beginning Analysis

15:05:55 NX NASTRAN Authorization Information - System Attributes
15:05:55 --------------------------------------------------------
15:05:55 Model: Intel(R) Xeon(R) CPU E5-1650 v3
15:05:55 Machine: Intel64 Family 6 Model 63 Steppi
15:05:55 OS: Windows 7
15:05:55 Version: Service Pack 1
15:05:55 License File(s): 28000@LocalHost

15:05:55 The FEMAP dll Search String is c:\femapv1132\auth_*.dll .
15:05:55 Found the FEMAP authorization dll auth_113.dll
15:05:55 Loading FEMAP Authorization dll auth_113.dll

15:05:55 NX NASTRAN Authorization Information - Checkout Successful
15:05:55 ----------------------------------------------------------
15:05:55 License for module NX Nastran Basic - FEMAP Desktop checked out successfully

16:43:58 Analysis started.
16:43:58 Geometry access/verification to CAD part initiated (if needed).

 

In this case analysis started after license checked out in more than 1,5 hours.

My model has about 600k elements and 1100k nodes. This analysis ran on computer with 64 GB RAM and Scratch on 1 TB SSD (OS and CPU see in log).

 

I ran this analysis of the same model on other computer too with 32 GB RAM and Scratch on 1 TB SSD. In this case part of log file was the following:

 

12:27:02 Beginning Analysis

12:27:02 NX NASTRAN Authorization Information - System Attributes
12:27:02 --------------------------------------------------------
12:27:02 Model: Intel(R) Core(TM) i7-3820 CPU @
12:27:02 Machine: Intel64 Family 6 Model 45 Steppi
12:27:02 OS: Windows 7
12:27:02 Version: Service Pack 1
12:27:02 License File(s): 28000@LocalHost

12:27:02 The FEMAP dll Search String is c:\femapv1132\auth_*.dll .
12:27:02 Found the FEMAP authorization dll auth_113.dll
12:27:02 Loading FEMAP Authorization dll auth_113.dll

12:27:02 NX NASTRAN Authorization Information - Checkout Successful
12:27:02 ----------------------------------------------------------
12:27:02 License for module NX Nastran Basic - FEMAP Desktop checked out successfully

15:24:42 Analysis started.
15:24:42 Geometry access/verification to CAD part initiated (if needed).

 

On this computer analysis waited 3 hours after license checked out.

 

What makes NX Nastran during this time? How can I avoid this? This happened with Femap v11.3.2.

 

Best regards,

 

Peter Kaderasz

4 REPLIES 4

Re: Long time until analysis starting in case of Bolt Preload on Solid type Bolt Region

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Peter,

The best advice: mesh bolts with CHEXA 8-nodes instead CTETRA 10-nodes solid elements, you will get an important model size reduction and this will reduce solution time.

In any case, the use of 3-D SOLID BOLTS instead 1-D bar/beam elements takes its time, the cost is important: the first is a local model, the other is global. With 3-D solid bolts you are able to investigate local effects in detail like contact between bolts & faces of the solid body, etc..

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Long time until analysis starting in case of Bolt Preload on Solid type Bolt Region

Gears Phenom Gears Phenom
Gears Phenom

Hello Blas,

 

I've made a modification in my model and remake the bolts to HEXA elements. In this case the part of my log file was the following:

 

11:11:50 Beginning Analysis

11:11:50 NX NASTRAN Authorization Information - System Attributes
11:11:50 --------------------------------------------------------
11:11:50 Model: Intel(R) Xeon(R) CPU E5-1650 v3
11:11:50 Machine: Intel64 Family 6 Model 63 Steppi
11:11:50 OS: Windows 7
11:11:50 Version: Service Pack 1
11:11:50 License File(s): 28000@LocalHost

11:11:50 The FEMAP dll Search String is c:\femapv1132\auth_*.dll .
11:11:50 Found the FEMAP authorization dll auth_113.dll
11:11:50 Loading FEMAP Authorization dll auth_113.dll

11:11:50 NX NASTRAN Authorization Information - Checkout Successful
11:11:50 ----------------------------------------------------------
11:11:50 License for module NX Nastran Basic - FEMAP Desktop checked out successfully

11:59:28 Analysis started.
11:59:28 Geometry access/verification to CAD part initiated (if needed).

 

In this case analysis started after about 40 min. waiting, but I think this is a long time too. What does NX Nastran in this time?

 

Best regards

 

Peter Kaderasz

Re: Long time until analysis starting in case of Bolt Preload on Solid type Bolt Region

Siemens Phenom Siemens Phenom
Siemens Phenom

You may not be getting the complete story from just the log file. Check or post the f04 file to see what Nastran is really doing (if anything) during that time. You can add DIAG 8,15 to get more complete information in the f04 file.

 

Regards,

 

Joe

Re: Long time until analysis starting in case of Bolt Preload on Solid type Bolt Region

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Just a shot in the dark but maybe your anti-virus software is interfering?