Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple license to install in single license server

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi all, 

 

Anyone can able to support on my question below,

 

My customer having 2 network licenses under single Host ID, They want both licenses to be install in single Server to distribue .

Is it possible to configure two licenses in one license server , how to do the settings in client machine to receive the license which is availble , while the other license used.

 

Kindly support on this.

 

Thanks & regards,

Anburajan

 

2 REPLIES 2

Re: Multiple license to install in single license server

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

If you mean two different products, like Femap and NX, then that should work fine as long as both license files are for that single server.  Just run the standard installations for each product.  Double check to make sure they use different port numbers, which they should by default.

 

If you mean two seats of Femap, that will work fine as long as they are in a single license file, and both are network seats of Femap.  A single Femap license file can have as many seats and options as you would like to buy, and then they can float around the network to whoever needs them.

 

If the Femap licenses are in two different license files, then you would want to combine them, and you would work with your Femap reseller to do that.

Re: Multiple license to install in single license server

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Thanks ChrisTeague . Good explanation .