Cancel
Showing results for 
Search instead for 
Did you mean: 

NOCOMPS

Valued Contributor
Valued Contributor

Where do I find the PARAM,NOCOMPS in FEMAP?

Thanks.

1 REPLY 1
Highlighted

Re: NOCOMPS

Siemens Phenom Siemens Phenom
Siemens Phenom

NOCOMPS is not one of the standard NASTRAN PARAMs that FEMAP supports in the GUI, you have to manually enter it.  In the Analysis Case Manager, open up the NASTRAN Bulk Data Options -

 

BulkOptions.jpg

Press the "Start Text" option...now enter any text you want to appear in the Bulk Data section of the NASTRAN input file -

PARAMNOCOMPS.jpg

As you can see here, you can enter any NASTRAN command you wish, as well as point to an include file with extra NASTRAN Bulk Data entries.

 

Regarding PARAM's like this, a full PARAM manager, where we catalog all available PARAM's and provide access to them is on the development short list.

 

Mark.