Re: NX Nastran quality check - HEX DETJ

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Karolina,

Using FEMAP V12 the NX NASTRAN quality check performs with success, see below:

 

Check Element Quality
2560 Element(s) Selected...
No Elements Outside of Maximum Allowable Value.

   Quality Check               Number Failed      Worst Value
      Hex AR                             0           3.555333
      Hex DetJ                           0         1.28827E-9
      Hex Warp                           0                 1.
 
   0 Elements Failed out of 2560 Checked.

check-quality.png

 

Curiously, after converting the model from meters to millimeters using command TOOLS > CONVERT UNITS we can see that the resulting value of HEX DetJ is different, changes from 1.28827E-9 to 1.28827, strange ..., this should be revised & investigated by FEMAP developers, the element quality check should be invariant of the model units used...

 

Check Element Quality
2560 Element(s) Selected...
No Elements Outside of Maximum Allowable Value.

   Quality Check               Number Failed      Worst Value
      Hex AR                             0           3.555333
      Hex DetJ                           0            1.28827
      Hex Warp                           0                 1.
 
   0 Elements Failed out of 2560 Checked.

check-quality-mm.png

 

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: NX Nastran quality check - HEX DETJ

Creator
Creator

Dear all,

Thanks for involving into the discussion, I will ask if it's possible to upgrade my Femap version.

Regards,

Karolina

Re: NX Nastran quality check - HEX DETJ

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

That should not happen. I will look into it.

Thanks

Re: NX Nastran quality check - HEX DETJ

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Nastran also exhibits the scaling behavior with Jacobians for solid elements. Nastran Jacobian and Femap Nastran DetJ report the same values. These are the expected results according to the Nastran developers. The values are not normalized and only become an issue with model accuracy when Nastran Jacobian is less than 0.0.