Highlighted

New Solid isn't selectable after Copy / Rotate / Reflect Solid commands

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I found an issue in Femap v11.4.0. I created a Solid in Layer 1, than activate Layer 2 and set Layer 2 to not visible. If I use Geometry / Copy, Rotate or Reflect commands with Match Original Color and Layer Generation Options, the newly created Solid will be not selectable until I set Layer 2 to visible. This mean that match layer work only for surfaces, curves and points of solid, but for solid not. New solids always created in active layer.

 

This is annoying for example, when I reflect a lot of solids in many layers, because after reflecting I must correct layers of all reflected solids to continue work.

 

In earlier versions after reflecting solids I could select new solids, only these solids war not shown if I moved mouse cursor over them. In Femap v11.4.0 I can't select either with single pick or box, circle pick method.

 

Best regards,

 

Peter Kaderasz

1 REPLY 1

Re: New Solid isn't selectable after Copy / Rotate / Reflect Solid commands

Siemens Phenom Siemens Phenom
Siemens Phenom

Thanks for alerting us to this problem. It has been fixed for the next release of FEMAP.