Showing results for 
Search instead for 
Did you mean: 

No temperature data for element



I am attaching an assembly for a steady state heat transfer analysis. The round part is a chip, the other is a radiator.

Set up:

1) Body load of 300K.

2) Heat flux (25W) from bottom face of chip to radiator via contacting surface.

3) Glued contact surface (Gluetype =1, Pentyp = 2, Normal Factor = 10000 , BGSET = .002)

4) Convection loss  (h=25, T = 300) from all surfaces of the radiator except contact surface with chip.


One of the errors I am getting is error 4017 - "There is no temperature data for an element in set"

Any ideas what is going wrong?