Cancel
Showing results for 
Search instead for 
Did you mean: 

Output of SOL601

Creator
Creator

Hello All,

 

I use SOL601 to make a nonlinear analysis with plastic strain. The model consists of hexa8 elements.

Is there any way to get from NX.Nastran in output set SOLID Elastic and Plastic Strain Components separatly?

For example, Ansys output has these components.

 

Yours sincerely,

Arcady

2 REPLIES 2

Re: Output of SOL601

Siemens Phenom Siemens Phenom
Siemens Phenom

SOL 601 reports the following strains for solid elements:

Nonlinear Solid X Normal Strain
Nonlinear Solid Y Normal Strain
Nonlinear Solid Z Normal Strain
Nonlinear Solid XY Shear Strain
Nonlinear Solid YZ Shear Strain
Nonlinear Solid ZX Shear Strain
Nonlinear Solid Max Prin Strain
Nonlinear Solid Min Prin Strain
Nonlinear Solid Int Prin Strain
Nonlinear Solid Max Shear Strain
Nonlinear Solid Mean Strain
Nonlinear Solid Von Mises Strain
Nonlinear Solid Plastic Strain

 

There is no output option to report the elastic portion separately.

 

Regards,

 

Joe

Highlighted

Re: Output of SOL601

Creator
Creator

Thanks you for the clarification.

 

Regards,

Arcady