Cancel
Showing results for 
Search instead for 
Did you mean: 

PGAP Preload in SOL 106 analysis

Dear Femap users,

 

I need to apply a bolt preload in a NL analysis (SOL106).

I saw that bolt preload is not inlcuded in this module, and then I would like to create this effect by mean of PGAP card.

I've performed some analysis but I see that this input data is not considered in the model.

There are other particular setting that I miss?

 

Thanks

Best regards

S.Milani

4 REPLIES 4

Re: PGAP Preload in SOL 106 analysis

Gears Phenom Gears Phenom
Gears Phenom

Rod/Beam (maybe CBUSH too) and material with thermal expansion coefficient - you freeze bolt so it tight two parts together. This is oldschool bolt preload. But you have to calculate bolt shortening by hands before analisys or make couple of runs to get desired preload value.

Re: PGAP Preload in SOL 106 analysis

Dear @Karachun,

 

I've already performed an analysis with this technique (thanks for your indication), but I would like to learn another method, and understand why PGAP option not work.

 

Thanks and best regards

 

S.Milani

Re: PGAP Preload in SOL 106 analysis

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Stefano,

Simply play with temperature to obtain the effect of bolt preloading: Strain = AlphaX • DeltaT, then compute the amount of DeltaT necessary to obtain the displacement caused by bold preload.

 

thermal_strains_theory.png

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: PGAP Preload in SOL 106 analysis

Dear @Blas_Molero,

 

thanks for your reply. I've already use this option with success in my model, but I saw that there 's also PGAP option, and I would like to understand how can I use it (my curiosity)!!

 

Thanks and best regards

S.Milani