Cancel
Showing results for 
Search instead for 
Did you mean: 

Postprocessing - Positive crossing doesn't have stress output

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello guys,

I have find a issue when I finished random analysis. There has stress result in "Positive crossing output" in previous version, but it's no stress result in current version. Should I type any command in input deck to request stress result for positive crossing? 

 

Thank you for your kindly help.

Kenshin

 

image001.jpg

1 REPLY 1

Re: Postprocessing - Positive crossing doesn't have stress output

Siemens Phenom Siemens Phenom
Siemens Phenom

The issue results from a change in the NXN 12 solver. The name of the datablock containing that information changed and therefore Femap does not read the data from op2 created with NXN 12. If you have Femap 11.4.2 and use the NXN 11.02 solver then you can read/attach that op2 in Femap 12.0 and you should see the stress data as expected. The issue has been reported and should be corrected in the next release.

 

Regards,

 

Joe