Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

SOL401 Nonlinear multistep and FEMAP

Valued Contributor
Valued Contributor

Is it possible to export an input file for SOL401 from FEMAP ?

 

I can't find an option for this solver in Analysis Set Manager.

1 REPLY

Re: SOL401 Nonlinear multistep and FEMAP

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Fergus,
The new NX NASTRAN MultiStep Nonlinear Solver (SOL401) native from SIEMENS will be supported in FEMAP after releasing NX Nastran V12, so hopefully it will be available at the end of the year 2017 (or most probably early 2018). At that time we will have a FEMAP product for NX NASTRAN (SOL401). Until then, FEMAP cannot set up the solve for it, sorry!.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/