Cancel
Showing results for 
Search instead for 
Did you mean: 

SOL701 STAMPING

Experimenter
Experimenter

Hi!
I'm new in SOL 701.
Now I am trying to simulate simple stamping process. You can see it on the picture below. I think the problem in material options, but can't understand where it hide.
 Solver gave me those output data

 

1.PNG

 

Here are the material settings

 

2.PNG3.PNG4.PNG

 

Tell me what I'm doing wrong.

 

best regards,

 

Yuliia

 

3 REPLIES 3

Re: SOL701 STAMPING

Siemens Phenom Siemens Phenom
Siemens Phenom

SOL701 is for very short duration dynamic events.  You should use either SOL601 Static or Transient.

Please refer to https://community.plm.automation.siemens.com/t5/3D-Simulation-Knowledge-Base/Sheet-Metal-Forming-wit...

 

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development

Re: SOL701 STAMPING

Siemens Phenom Siemens Phenom
Siemens Phenom

Did you apply the load as a time-based load?

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development

Re: SOL701 STAMPING

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello!

Unless your stamping velocities are very high, these stamping problems can usually be modelled as a static nonlinear problem. In your case, can you try SOL 601,106 instead of SOL701?

 

When defining your step, make sure you use enough increments per step to ensure convergence in the Newton-Raphson solver. (Solver options)

Cheers,

Jacques.