Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Solid Equivalent for Offset/Washer Tool

Valued Contributor
Valued Contributor

Is there an solid equivalent for the offset curve/washer tool that will slice out an annular cylinder around an existing hole?

 

I am meshing a part that has holes in surfaces with compound curvature, and I am trying to core out solids bounding the holes to create uniform boundary layers of elements around the holes. Currently, I am having to manually extrude cylindrical surfaces that are concentric with the hole cylinder and use these surfaces to slice the body. Unfortunately, I have many holes and this is very tedious. In many cases, the guide curves of the hole surface and extruded surfaces are clocked at different angles, causing problems for meshing.

12 REPLIES 12

Re: Solid Equivalent for Offset/Washer Tool

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

How about using the Meshing Toolbox to put a washer surface around each hole quickly.  Then use <Geometry><Solid><Embed Face...>?  That will create the cylindrical solids you are looking for.

Re: Solid Equivalent for Offset/Washer Tool

Valued Contributor
Valued Contributor

Unfortunately, that doesn't really work for me with the geometry I'm dealing with because the forward and rear surfaces are not parallel and are not perfectly perpendicular to the hole. Also, creating a washer doesn't work consistently because the edge of the hole is ovular rather than circular.

 

The method I've been using so far has been locating the working plane normal to the hole axis, drawing a circle, and extruding the circle as a surface to slice the body. This is just very tedious, and I can't always locate the central axis of the hole very well.

Re: Solid Equivalent for Offset/Washer Tool

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Have a look at Mark Sherman's post on offset curves.  It should be able to do what you are looking for.

https://community.plm.automation.siemens.com/t5/3D-Simulation-Femap-Forum/Adding-a-pad-to-non-circul...

 

Re: Solid Equivalent for Offset/Washer Tool

Valued Contributor
Valued Contributor

This is marginally closer, but still not quite what I'm looking for. I am looking for something that will not merely offset the curves but actually create a spliced solid that is offset from a hole. My ultimate aim here is to be able to create a uniform hex mesh boundary around a hole. The Offset Curve/Washer tool is really only useful for membrane-type meshing.

Re: Solid Equivalent for Offset/Washer Tool

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Once you have the offset curves you should be able to use the <Geometry><Solid><Embed Face...> command and that will give you the solids you are looking for.  It might be helpful to perhaps post a picture or two of the geometry in question - or maybe a sample of the geometry if confidentiality allows...

Re: Solid Equivalent for Offset/Washer Tool

Valued Contributor
Valued Contributor

Unfortunately, I do not believe I can share the geometry.

 

I do have another idea, but I could use some help, as I'm only an intermediate scripter. I have written a script to create lines through the axes of cylindrical surfaces. Ideally, I could expand the script to create a cylinder around these axes with a user specified radius/diameter. I have been looking through the Femap API documentation but there does not seem to be an object method or function that directly performs the same thing as <Geometry><Surface><Cylinder...>. Am I missing something?

 

Here is the script as is, for reference:

 

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim surf As femap.Surface
    Set surf = App.feSurface

    Dim surfSet As femap.Set
    Set surfSet = App.feSet

    Dim skippedSet As femap.Set
    Set skippedSet = App.feSet

    Dim rad As Double
    Dim aLength As Double
    Dim cBase As Variant
    Dim nBase(2) As Variant
    Dim aVect As Variant
    Dim cEnd(2) As Variant
    Dim pOffset As Double

    Dim tracker As femap.TrackData
    Set tracker = App.feTrackData

    Dim cTrack As femap.Set
    Set cTrack = App.feSet

    Dim checkTol As Double

    Dim rc As Long

    ' Begin tracking created curves
    tracker.Start(4)

    ' Select cylindrical surfaces
    rc = surfSet.Select(FT_SURFACE, True, "Select cylindrical surfaces to create Axes")
    If rc = FE_NOT_EXIST Then
        App.feAppMessage(FCM_ERROR, "One or more surfaces do not exist")
        Exit Sub
    ElseIf rc = FE_CANCEL Then
        Exit Sub
    End If

    ' Prompt user to select length of axis and where to center
    Begin Dialog UserDialog 270,105,"Axis Length" ' %GRID:10,7,1,1
        text 30,14,100,21,"Axis length",.Text1
        text 30,42,100,14,"Percent Offset",.Text2
        TextBox 140,14,100,14,.axisLength
        TextBox 140,42,100,14,.offsetValue
        OKButton 20,70,100,28
        CancelButton 140,70,100,28
    End Dialog
    Dim dlg As UserDialog
    Dialog dlg

    ' Check axis length
    If IsNumeric(dlg.axisLength) Then
        aLength = CDbl(dlg.axisLength)
    Else
        App.feAppMessage(FCM_ERROR, "Axis length must be a numeric, non-zero value.")
        Exit Sub
    End If

    ' Check for baseOffset option and offsetValue
    If dlg.offsetValue = "" Then
        pOffset = 0.0
    ElseIf IsNumeric(dlg.offsetValue) = False _
      Or CDbl(dlg.offsetValue) > 1.0 _
      Or CDbl(dlg.offsetValue) < 0.0 Then
        App.feAppMessage(FCM_ERROR, "Offset must be a value >=0 and <=1.")
        Exit Sub
    Else
        pOffset = CDbl(dlg.offsetValue)
    End If

    ' Create axis base point and vector
    Do While surf.NextInSet(surfSet.ID)
        If surf.Cylindrical(rad, cBase, aVect) = FE_FAIL Then
            skippedSet.Add(surfSet.CurrentID)
        Else
            ' Determine end points for axis
            For i = 0 To 2
                nBase(i) = cBase(i) - aVect(i) * aLength * pOffset
                cEnd(i) = cBase(i) + aVect(i) * aLength * (1 - pOffset)
            Next i

            ' Create line
            App.feLinePoints(False, nBase, cEnd, False)
        End If
    Loop

    ' Set from created curves
    tracker.Stop(4)
    tracker.Created(4, cTrack.ID, False)

    ' Merge created coincident points and curves
    checkTol = 0.01 * aLength  ' check tolerance as 1% of specified axis length
    App.feCheckCoincidentCurve(cTrack.ID, checkTol)

    App.feAppMessage(FCM_NORMAL, cTrack.Count() & " curve(s) created...")

    If skippedSet.Count() > 0 Then
        App.feAppMessage(FCM_ERROR, skippedSet.count() & " surfaces were non-cylindrical and skipped.")
    End If

End Sub

Re: Solid Equivalent for Offset/Washer Tool

Siemens Creator Siemens Creator
Siemens Creator
Sub Main
	Dim App As femap.model

	Dim curveSet As femap.Set
	Dim surfacesOfCurve As femap.Set
	Dim firstSurfaces As femap.Set
	Dim secondSurfaces As femap.Set
	Dim surfacesNew As femap.Set

	Dim surfaces1 As femap.Surface
	Dim surfaces2 As femap.Surface
	Dim surfaceToCheck As femap.Surface

	Dim curve1 As femap.Curve

	Dim vBase As Variant, vNormal As Variant, vCenter As Variant

	Dim rc As Integer

	Dim curveID As Long, washerMode As Long, offsetModeFactor As Long
	Dim planarSurfaceOfCurve As Long, faceSurfaceID As Long

	Dim washerFactor As Double

	Dim autoSelect As Boolean, saveSplit As Boolean, extendCurvesToClosestEdge As Boolean

	Set App = feFemap()

	Set curveSet = App.feSet
	Set surfacesOfCurve = App.feSet
	Set firstSurfaces = App.feSet
	Set secondSurfaces = App.feSet
	Set surfacesNew = App.feSet

	Set surfaces1 = App.feSurface
	Set surfaceToCheck = App.feSurface

	Set curve1 = App.feCurve

	washerMode = 1
	offsetModeFactor = 0
	washerFactor = 1.0
	autoSelect = False
	saveSplit = True
	extendCurvesToClosestEdge = True

	surfaces1.Reset
	While surfaces1.Next()
		rc = firstSurfaces.Add(surfaces1.ID)
	Wend

	rc = surfacesNew.Copy(firstSurfaces.ID)

	rc = curveSet.SelectID(FT_CURVE, "Select Curve for Washer", _
			curveID)

	rc = curve1.Get(curveID)
	rc = curve1.Center(vCenter)

	rc = curveSet.Add(curveID)

	rc = surfacesOfCurve.AddRule(curveID, FGD_SURFACE_BYCURVE)

	surfacesOfCurve.Reset
	While surfacesOfCurve.Next()
		rc = surfaceToCheck.Get(surfacesOfCurve.CurrentID)
		rc = surfaceToCheck.Planar(vBase, vNormal)
		If rc = FE_OK Then
			faceSurfaceID =surfacesOfCurve.CurrentID
		End If
	Wend

	rc = App.feCurveOffsetCurveWasher2(curveSet.ID, _
				faceSurfaceID, washerMode, _
				autoSelect, saveSplit, extendCurvesToClosestEdge, _
				washerFactor, offsetModeFactor)

	Set surfaces2 = App.feSurface

	surfaces2.Reset
	While surfaces2.Next()
		rc = secondSurfaces.Add(surfaces2.ID)
	Wend

	rc = surfacesNew.AddNewRemoveCommonSet(secondSurfaces.ID)

	surfacesNew.Reset

	rc = App.feSolidEmbedFace(faceSurfaceID, 0, 1, 0., 0., True)
	rc = App.feSolidEmbedFace(surfacesNew.First, 0, 1, 0., 0., True)

End Sub

Re: Solid Equivalent for Offset/Washer Tool

Genius
Genius

Create the circles (one per hole location), then project them onto the surfaces with the meshing toolbox/geometry editing/project curve. They won't be perfect circles anymore, but close enough. Then try using <Geometry><Solid><Embed Face...> as Chris suggested.

Re: Solid Equivalent for Offset/Washer Tool

Valued Contributor
Valued Contributor

That's what I've been doing thus far. I'm just looking for something that would be more expedient than manually locating the work plane, drawing a circle, projecting it to a surface, and then embedding the face. It's fine for one to two holes, but gets cumbersome when you have many holes.