Starting the Direct Matrix Abstraction Program (DMAP) from Femap with Nastran

Not applicable
How I can to start the Direct Matrix Abstraction Program (DMAP) from Femap with Nastran?
1 REPLY 1

Re: Starting the Direct Matrix Abstraction Program (DMAP) from Femap with Nastran

Innovator
Innovator
Hello!,
DMAP (Direct Matrix Abstraction Programming) is a high-level programming language that is available in NX NASTRAN.
All solution sequences in NX NASTRAN are comprised of DMAP statements. Any solution sequence may be listed by inserting COMPILER LIST into the Executive Control Section of the NX NASTRAN input file.
DMAP alters allow you to modify any solution in NX NASTRAN.
DMAP is not part of the FEMAP with NX NASTRAN BASIC bundle, requires an additional license.
Best regards,
Blas.