TMG Error with missing geometry in thermal coupling

When I try to start a TMG solve, I get an error saying that I have thermal coupling missing geometry. However, the message does NOT say which thermal coupling is giving me trouble. Instead it just says "The following entities reference empty geometry" with Thermal Coupling: (weird symbol). I attached a picture of the error message. 

 

In the past it would list the name of the thermal coupling, but now it's the symbols shown in the picture. Without knowing which TC is being problematic, I'm forced to add/remove each one from study to guess and check. How do I fix this?

 

Thanks in advance for your help!

 

2 REPLIES 2

Re: TMG Error with missing geometry in thermal coupling

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

What version of FEMAP are you using? Do you have special characters in your TC names or group names?

Jacques

Re: TMG Error with missing geometry in thermal coupling

It's FEMAP 11.3.1 and no, all of my naming is with normal characters.