Cancel
Showing results for 
Search instead for 
Did you mean: 

Trial version looking for a dongle

Not applicable
when installing i missed the button to change from a dongle based to a trial version. How do i get back to that point
1 REPLY 1

Re: Trial version looking for a dongle

Innovator
Innovator
Hello!,
You are running Femap under the wrong licensing scheme (the Network Client option should be selected during installation). To fix this, run a file called go_network.bat in the Femap install directory (make sure that Femap is not running at the time). This will change the authorization dll from the Nodelocked Dongle version to the Network Client version. You will not need a new license, your current one will still work.
Best regards,
Blas.