Showing results for 
Search instead for 
Did you mean: 

Version control of analysis


In the coding world, tools like git or svn are used for efficient version control (that is, the life cycle of the code is saved and is accessible within a nice interface). Is there a way to do this for FEMAP analyzes? You can use git, for instance, on the FEMAP .modfem files, but git only has limitted functionality on these bindary files. Right now, I just save the files with incremental file names, but this is less than ideal. Thoughts?