Highlighted

Which mesh should i use?

Experimenter
Experimenter

Hello All,

Im new user of FEMAP.im trying to mesh taper pin using hex meshing,but it shows error massage like Solid 1 can not be hex meshed. Unable to identify the surfaces for the base and top of the mesh.

Can anyone please help me

 

I attached model herewith.

 

 

Amol☺☺

3 REPLIES 3

Re: Which mesh should i use?

Experimenter
Experimenter

attached is model

Re: Which mesh should i use?

Siemens Phenom Siemens Phenom
Siemens Phenom

FEMAP requires that you split a solid down in to "sweepable" regions for hex meshing.  For your part, I divided it down into 16 solids.  I used mosly - Geometry - Solid - Embed Face. 

P55_Subdivided.jpg

When you "size" the geometry for hex meshing, FEMAP will automatically determine the sweeps, and the connected faces to make sure all the nodes are merged, here's the resulting mesh -

 

P55_HexMesh.jpgI

 

I have attached the split-down Parasolid file.

 

Mark.

Re: Which mesh should i use?

Experimenter
Experimenter
Thak you Mark...☺☺