Cancel
Showing results for 
Search instead for 
Did you mean: 

embed solid

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

hi,

 

i have 4 parts. after embed solid, in tree i have only one part (solid)

how to get back the remaining solids (parts)?

embed.JPGbefore embed solidafter.JPGafter embed solid

6 REPLIES

Re: embed solid

Siemens Legend Siemens Legend
Siemens Legend

Shreeharsha1,

 

Could you help illustrate what is happening with some pictures? And what exact commands are you using?

 

 

Re: embed solid

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

@T_Giampietro

HI,

 

command which i am using is geometry-solid-embed

the output what i am getting is here in pic.

berore_embed.JPGbefore embedafter_embed.JPGafter embed

please find the attached cad model for your reference.

 

regards,

shreeharsha

Re: embed solid

Siemens Legend Siemens Legend
Siemens Legend

What exactly are you trying to accomplish?

 

I believe Geometry > Solid > Embed is used more for the method of when you create/move a solid within/overlapping the volume of  another existing solid. After the command is run the solid volume within the bigger solid will be removed from the bigger. 

 

Simple example:

1. Created solid cube

Full Solid.JPG

 

2. Created cylinder within the volume of the cube
Full Solid2.JPG

 

Shown together-
Solids Shown Together.JPG

3. After command and hiding the cylinder
After Embed.JPG

 

 

 

Re: embed solid

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

@T_Giampietro

 i am trying to create fluid mesh..

 

Re: embed solid

Siemens Legend Siemens Legend
Siemens Legend

To do that you will want to use the command Geometry >  Solid > Fill Hole. Select an inner curve on the solid "case". 

Fill Hole.JPG

Now there is another solid within the "case" solid. Note the geometry list in Model Info

Filled Hole.JPG

 

Now you will want to use the command Geometry > Solid > Embed. Select the newly created solid. Then select one of the inner three solids (2. pcb 3. chip 4. chip2 ). Repeat twice for the other two inner solids. 

 

This will leave all solids. 

For liquid mesh.JPG

 

 

Re: embed solid

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

@T_Giampietro

thank you. got it.

 

but one more question i have?

 

if i project a circle on the front face of the embed body (case), i cant able to apply tetra mesh to that. it is prompting like only single surface boundaray required?

then how to combine the project circle face with embed body?

 

 

 

regards,

shreeharsha