Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

feMeshDetach "parameter requires expression"

Valued Contributor
Valued Contributor

Has anyone used the `feMeshDetach` API function? It keeps kicking out an error for me that isn't very helpful:

 

API Error (Line 75): Parameter requires an expression.
         rc = App.feMeshDetach(FT_NODE, nSet.ID, 0)--> 

Here is my script. It moves nodes onto a surface with the option of associating the nodes to the surface after they've been relocated. It works perfectly if the nodes are not associated with anything and I remove the line calling for them to be detached from their existing geometry.

 

 

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    App.feAppMessage(FCM_COMMAND, "Move Nodes onto Surface")

    Dim rc As Long

    ' point set
    Dim nSet As femap.Set
    Set nSet = App.feSet

    ' surface to project onto
    Dim s As femap.Surface
    Set s = App.feSurface

    ' dummy point object
    Dim n As femap.Node
    Set n = App.feNode

    Dim success As Long
    Dim attach As Boolean
    Dim n_count As Long
    Dim attach_id() As Long
    Dim attach_type() As Long
    Dim n_array As Variant

    ' prompt user to select nodes
    rc = nSet.Select(FT_NODE, True, "Select nodes...")
    If rc = FE_OK Then
        n_count = nSet.Count()
        ReDim attach_id(n_count)
        ReDim attach_type(n_count)
    ElseIf rc = FE_NOT_EXIST Then
        App.feAppMessage(FCM_ERROR, "Selected nodes do not exist.")
    ElseIf rc = FE_CANCEL Then
        Exit Sub
    End If

    ' prompt to select surface
    rc = s.SelectID("Select surface to project onto...")
    If rc = FE_NOT_EXIST Then
        App.feAppMessage(FCM_ERROR, "Selected surface does not exist.")
    ElseIf rc = FE_CANCEL Then
        Exit Sub
    End If

    ' Choose whether or not to attach nodes to surface
    rc = App.feAppMessageBox(3, "Associate nodes with surface?")
    If rc = FE_OK Then
        attach = True
    ElseIf rc = FE_FAIL Then
        attach = False
    Else
        Exit Sub
    End If

    ' move nodes onto surface
    success = 0
    Do While n.NextInSet(nSet.ID)
        rc = App.feProjectOntoSurface(FT_NODE, nSet.ID, s.ID)
        If rc = FE_OK Then
            attach_type(success) = FT_SURFACE
            attach_id(success) = s.ID
            success = success + 1
        End If
    Loop

    App.feAppMessage(FCM_NORMAL, Cstr(success) & " nodes moved onto surface...")

    ' associate nodes with surface
    If attach Then
        nSet.GetArray(n_count, n_array)

App.feMeshDetach(FT_NODE, nSet, 0) rc = App.feMeshAttachNodes(n_count, n_array, attach_type, attach_id) If rc = FE_OK Then App.feAppMessage(FCM_NORMAL, Cstr(success) & " nodes associated with surface...") End If End If End Sub

 

2 REPLIES 2

Re: feMeshDetach "parameter requires expression"

Gears Legend Gears Legend
Gears Legend

Hello,

 

I think feMeshDetach requires more parameter. See 3.10.5.4 in Femap Help.

 

Try 

rc = App.feMeshDetach(FT_NODE, nSet.ID, 0, 0, False)

I use in my API the following without error:

rc=App.feMeshDetach( FT_NODE, nodeSet.ID, FT_CURVE, curveID, False)

Best regards

 

Peter Kaderasz

Re: feMeshDetach "parameter requires expression"

Valued Contributor
Valued Contributor

That did it! I misinterpreted the help descriptions of the last two arguments to mean that if you put 0 in for attachTYPE, that they are not used.