how to save.modfem file from parasolid imported file

Experimenter
Experimenter

 i  imported model as parasolid and did analysis. but i was not able to see this resut, which format it stay*?  is it possible to save parasolid file directly to .modfem file.

 

 

2 REPLIES 2

Re: how to save.modfem file from parasolid imported file

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Sharuvai,

I don't understand very well the question, but I will give you the explanation of BASIC concepts to see if it can help you:

 

  • Parasolid is a format to import only geometry, not FEA data. FEMAP native database format has the extension *.modfem. If you create a Finite Element model in FEMAP the native file format is *.modfem.
  • FEMAP allows you to import a CAD model geometry using Parasolid (*.X_T format), then next you can save your FEMAP model as *.modfem.
  • CAD packages do not export directly the FEMAP format (*.modfem), simply export geometry that can be imported as well in FEMAP using STEP, Parasolid, IGES, ACIS, etc.. formats.
  • Please note that FEMAP can import Finite Element data from most of the FEM/FEA codes of the market, not only the input file but results as well. The main mission of FEMAP is to create finite element models, launch the FE solver, and postprocess results.

IMPORT-ANALYSIS.png

 

Please elaborate more your question to see if we can help you better, thanks!.

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: how to save.modfem file from parasolid imported file

Experimenter
Experimenter

thank you Smiley Happy