Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

how to see torsion when a moment is applied

Creator
Creator

Hello there!

I'm having a problem analysing a torsion.

I have a hollow NACA 0012 wing profile with a small slot on the trailing edge. I fully constrained one side and applied a moment on the other. I'm looking for the rotation values on the Z axis (preferably with the referencial on the centroid). It's expected that the torsion grows from 0 on the constrained side and maximum on the other side.

 

I'm using 2D elements with 1 mm thickness.

 

What am I getting wrong?

 

Thanks in advance 

 
Captura de ecrã 2018-06-14, às 19.50.48.jpg

2 REPLIES 2

Re: how to see torsion when a moment is applied

Phenom
Phenom

Looks like a question for the NX or Simcenter Forums, not the Femap forum, though there may be some people here who use both.

Re: how to see torsion when a moment is applied

Creator
Creator
Thanks, I posted it there as well!