Cancel
Showing results for 
Search instead for 
Did you mean: 

"Add Related Entities" command excluded CBUSH coordinate system?

Creator
Creator

Hello,

 

I'm using Femap 11.2 and ran into an issue with getting all the related entities into a group, specifically CBUSH's orientation coordinate system.  Here are the steps that led to my issue:

- Created a group with just the elements

- "Add Related Entities" command

- All the nodes related CSYS are added to the group, but not the CBUSH's CSYS that used to define its orientation

 

I don't remember running into this issue using an ealier version of Femap.  This is frustrating because I used a Referenced Group that comprise of many parts and keep getting fatal errors because a CBUSH's CSYS did not get into the group that is being analyzed.

 

Thanks,

Linh Bui

1 REPLY 1

Re: "Add Related Entities" command excluded CBUSH coordinate system?

Siemens Phenom Siemens Phenom
Siemens Phenom

The orientation of CBUSH via a Coordinate System is a relatively new feature and unfortunately incorporating this into "Add Related" was never implemented. This capability however will work in the upcoming v11.3 release.