Cancel
Showing results for 
Search instead for 
Did you mean: 

Element Visual Inspection

Community Manager Community Manager
Community Manager

When Femap finishes meshing a model a brief report of the mesh quality is written to the Messages pane.  However, often it’s desirable to visually inspect the worst elements of the mesh, and review their shape, and location in the model, an action which is not necessarily that easy to do with a solid model?

 

However, in Femap’s interactive Meshing Toolbox there is a locator function, which can be used to locate problematic geometry entities – curves and surfaces – as well as elements.

07_01.jpg

 

To switch on the Locator, first activate the Meshing Toolbox by clicking the Meshing icon in the Panes toolbar, and click on the Toggle Entity Locator icon on the Meshing Toolbox. Select Elements as the Search For criteria and Quality as the Search Method, and you will see all of the elements that fail the selected quality type and value.

 

Here Femap displays the transparent model, with the elements that failed the quality criterion highlighted.

 

07_02.jpg

 

Zooming up allows you to get a good view of the failed elements, and you can then make a decision based on the element shape and its location in the model whether or not it’s necessary to improve the mesh. If it is, then it’s easy to go back and use Femap’s Meshing toolbox to interactively change some of the meshing parameters in this area and improve the mesh.

 

(view in My Videos)