Cancel
Showing results for 
Search instead for 
Did you mean: 

Femap Tips and Tricks: Create Elements between Coincident Nodes

Community Manager Community Manager
Community Manager

The task of creating elements such as springs or gaps between coincident node points can present some challenges. For example, how do you pick the coincident node points individually? Femap offers a couple of solutions to help you create elements like these more easily.

 

To enable you to choose between coincident nodes, in a model that contains coincident nodes, click the right mouse button in the graphics area and select Pick Query.

 

17_01.jpg

 

So when you pick coincident nodes, the Select dialog appears allowing you to choose which one to pick.

 

17_02.jpg

 

Alternatively, you can use a shortcut key to make use of the Pick Query command on the fly. Right click in the graphics are and select Pick Normal to reset the picking method.

 

Enter the Control-E shortcut key to bring up the Define element dialog, click on the Type… button and select Spring/Damper as the element type to define a spring element (like CBUSH). Now pick as set of coincident nodes, and the first node will be populated in the dialog. Now hold down the Alt key and clicking on the coincident nodes a second time, the Select dialog appear, allowing us to choose the second coincident node.

 

17_03.jpg

 

However, you have many elements to create between coincident nodes, so you can use a more automated approach and create them all in one single command.

 

Select the menu command Mesh / Connect / Coincident Link. Select all the nodes to be considered, enter a value for the Coincident Tolerance, or leave the default value and click OK.

 

17_04.jpg

 

Complete the definition for the connecting element properties in the Generate Connection Options dialog, and click OK to create all of the connecting elements at once.

 

17_05.jpg

 

 

 

 

(view in My Videos)