Cancel
Showing results for 
Search instead for 
Did you mean: 

Femap Tips and Tricks: Model Info Tree Shortcuts

Community Manager Community Manager
Community Manager

Long lists of entities like Materials or Properties are easier to navigate using the Model Info entity scrolling capability. You can set the maximum number of entities to display in File / Preferences; in the Model Info section of the User Interface tab you can specify Max Entities.

 

Femap Model Tree Shortcuts

 

In the Model Info tree, if the number of entities of a particular type exceeds the Max Entities value, then Previous and Next entries will appear at the top and bottom of that branch of the tree.

 

Femap Model Tree Shortcuts

 

You can Click on Next or Previous to scroll through the list of entities like properties or materials. You can also use Control and Shift with the middle mouse wheel to move to the next defined selection or visible selection, and Control and Shift together to move right to the bottom or top of the list.

 

Femap Model Info Tree Shortcuts

 

Also in the Model Info tree you can quickly set up load and constraint sets using the Copy To Set and Move To Set commands which can be accessed by right-clicking on Load Definitions.

 

Femap Model Info Tree Shortcuts

 

Femap Model Info Tree Shortcuts

 

Femap Model Info Tree Shortcuts

 

 

(view in My Videos)