Geometry Modification in Femap 11.2

Community Manager Community Manager
Community Manager

Femap 11.2 introduces new geometry modification tools that allow you to edit geometry entities interactively, including closing modeling gaps that typically occur following a mid-plane extraction command. You can interactively correct or repair problematic or incorrectly defined geometry as well. The Geometry Solid Slice commands available in previous versions of Femap have been consolidated to provide simpler execution and expanded functionality, and you can now slice solids using surface or curve geometry as cutting tools.

 

These four videos will provide more information on the following:

  • Mid-surface Extraction
  • Geometry Cleanup
  • Meshing
  • Geometry Updates

 

Mid-surface Extraction

 

 

 

Geometry Cleanup

 

 

 

Meshing

 

 

 

Geometry Updates